Humanoid robotics and an emerging sweet spot for GaN FETs

Artificial intelligence may determine what a humanoid robot can do, but actuator technology determines how effectively it can do it. Humanoid robotics represents one of the most demanding frontiers in modern automation. While humans walk across uneven terrain, climb stairs and maintain balance almost effortlessly, achieving the same capability in a humanoid robot is far more complex. Every step, lift, reach and balance correction requires dozens of motors to continuously accelerate, brake and adjust position in real time, all while drawing energy from the limited onboard battery that also powers AI processing, vision systems, sensors and communications.

Beneath the smooth outer shell of a typical humanoid robot, 20 to 40 brushless DC motors are distributed across its legs, torso, arms and hands. Some must deliver the torque required for standing, walking and balance recovery, while others provide the precise, responsive control needed for wrist, hand and finger movement. The electronics driving those motors must regulate torque in fractions of a second, often inside joints with barely enough room for the motor itself.

Unlike fixed industrial robots, humanoids carry their own battery, power electronics and cooling system. Every watt dissipated in an actuator reduces available runtime, while every cubic centimeter occupied by the inverter competes with batteries, sensors and computing hardware.

Not all joints are created equal

The requirements placed on a humanoid's actuators can vary dramatically throughout the robot. Hip and knee joints must handle high peak torques during walking, climbing and balance recovery, while wrist, hand and finger actuators place greater emphasis on compactness, responsiveness and precise motion control. Supporting everything from precision finger movements to kilowatt-class leg joints, while maintaining efficiency, compactness and thermal performance, creates a unique engineering challenge.

Typical number of joints and power requirements
Typical number of joints and power requirements

While the mechanical requirements of each joint differ, many humanoid designs share a common electrical architecture: a centralized 48-60 V battery feeding distributed three-phase motor drives, AI processors, sensors and communications systems. Designers must also account for switching transients, regenerative braking, cable inductance and system-level voltage margins. As a result, power devices in the 80-200 V range are becoming increasingly attractive, occupying a space between traditional low-voltage motor drives and high-voltage industrial inverters.

Simplified share a common electrical architecture
Simplified share a common electrical architecture

Most humanoid actuators use field-oriented control (FOC) to regulate motor current and torque. The effectiveness of FOC depends on accurate current feedback and predictable inverter behavior, particularly during rapid changes in load. In high-dynamic applications such as walking, balance recovery and object manipulation, the motor drive must respond quickly while minimizing losses and heat generation. These requirements place increasing demands on the power semiconductors used within the inverter.

Why GaN fits humanoid robotics

The combination of strict energy budgets, compact actuator packaging and demanding dynamic performance requirements aligns closely with the strengths of GaN technology. From highly integrated low-voltage motor drives used in compact actuators to medium-voltage solutions intended for higher-power joints, GaN offers designers additional flexibility when optimizing efficiency, power density and control performance.

GaN transistors combine low on-state resistance with fast switching capability and low charge-related losses. In a properly optimized inverter, this can reduce power dissipation or create room to increase PWM frequency without the switching-loss penalty typically associated with conventional silicon devices. Lower losses simplify thermal management, while higher switching frequencies can reduce current ripple and support smoother torque production, particularly when a robot is making the small, continuous corrections needed to maintain balance or manipulate an object.

Matching low-voltage and medium-voltage devices to the actuator

However, no single technology or voltage class will suit every actuator. Device selection should therefore begin with the actuator's motion profile rather than a single datasheet parameter. Peak torque, RMS phase current, PWM frequency, available cooling and acceptable current ripple all influence whether a low-voltage or medium-voltage GaN device is the best fit for a given actuator. Engineers should also evaluate efficiency and thermal behavior under both continuous operation and transient conditions, rather than assuming that the lowest RDS(on) specification will automatically deliver the best overall system performance.

Package technology plays an important role. In densely packed actuators, package parasitics and thermal performance can be just as important as the transistor's headline RDS(on). Top-side-cooled (TSC) packages help designers make better use of limited PCB area while providing an efficient thermal path, enabling compact motor-drive implementations that can benefit from GaN's switching performance. While thoughtful copper layout and heat spreading remain essential to achieving the intended performance, designers should make the comparison at inverter level: total loss, temperature rise, switching waveform and occupied PCB area under representative motion cycles.

Higher-power joints such as the hips, knees and waist may benefit from compact, high-dynamic-response inverters using 100 V or 200 V devices, particularly when regenerative energy and switching transients are considered. Here, Nexperia's medium-voltage GaN FETs in TSC packages (WQFN7 and UQFN5) offer an attractive combination of voltage headroom, switching performance and compact implementation. In practice, the required voltage margin is determined by real operating conditions, including regenerative events and measured overshoot, rather than the nominal battery voltage alone.

In contrast, compact actuators in the wrists, hands and fingers often place greater emphasis on PCB area, thermal management and control precision, making Nexperia’s low-voltage GaN FETs a compelling option, provided the maximum bus voltage and transient conditions remain within the device rating. The combination of low losses and a small power-stage footprint is especially attractive in these space-constrained applications.

From efficient switches to more capable robots

Dead time is also a necessary part of inverter operation, preventing shoot-through events in power stages. Excessive dead time can introduce additional losses, current distortion and torque ripple. The negligible reverse-recovery behavior of GaN devices allows designers to significantly reduce dead-time intervals. Experimental testing on a GaN-based motor-drive platform has demonstrated stable operation with dead times below 30 ns in high-current systems (see Enabling high-efficiency 48 V motor drives with GaN: diode-less operation and ultra-short dead time in 70 A / 100 kHz systems).

This evaluation work on a 48 V GaN-based three-phase inverter also demonstrated stable operation at switching frequencies up to 100 kHz and phase currents up to 70 A while maintaining efficiencies above 96%. Such performance highlights the potential of GaN for compact, high-performance motor drives where both efficiency and dynamic response are critical.

Making the balancing act look effortless

For actuator designers, the objective is not merely faster switching but smoother control and more efficient use of the available energy budget. Consider the repeated sequence of a walking robot. One leg accelerates while the other absorbs energy during deceleration, and multiple joints continuously exchange mechanical and electrical power. During braking, energy may be returned to the DC bus, making power-conversion efficiency and transient management increasingly important. When this cycle is repeated across dozens of actuators, even small improvements in inverter efficiency can have a meaningful impact on the overall energy budget.

Humanoid robots have effectively created a new class of motor-drive challenge. Supporting everything from highly articulated fingers to kilowatt-class leg joints from the same 48-60 V battery system creates an emerging sweet spot for GaN technology. From compact low-voltage solutions used in precision actuators to medium-voltage devices for higher-power joints, Nexperia enables designers to optimize efficiency, power density and dynamic performance across the robot.

 

Download our whitepaper - Enabling high-efficiency 48 V motor drives with GaN: diode-less operation and ultra-short dead time in 70 A / 100 kHz systems