Modernizing Power Path Design: Replacing Schottky Diodes or FETs with Integrated Ideal Diode Devices

Schottky diodes are widely used in commercial, automotive, and industrial electronics due to their fast-switching speed, efficiency, and reliability. They are often found in battery-powered gadgets, consumer electronics, and power supplies, where they provide robust protection.

The appeal of Schottky diodes, compared to traditional diodes, lies in their fast-switching characteristics and lower forward voltage drop, which help reduce power dissipation and heat generation. This reduction is essential for maintaining efficiency and protecting sensitive components. Like traditional diodes, Schottky diodes can prevent damage from miswiring through reverse polarity protection, and their ability to clamp voltage transients makes them a strong choice for robust system design and electrical fault protection.

 Figure 1. Power Management with Schottky diode
Figure 1. Power Management with Schottky diode

However, even with their lower forward voltage drop, Schottky diodes still introduce power loss, which can become significant—especially at higher currents. Their physical size and heat dissipation requirements can substantially increase the overall form factor needed to meet thermal constraints.

Modern designs often incorporate PMOS transistors to address these limitations, which significantly reduce power loss due to their very low forward conduction voltage and low RDS(ON). However, their limitations include a lack of reverse current blocking, making them unsuitable for power OR-ing when multiple power sources are present.

Figure 2. Power Management with PMOS FET
Figure 2. Power Management with PMOS FET

The benefits of Integrated Ideal Diodes

Integrated Ideal diodes represent the best of both worlds by combining the low power loss and forward voltage drop of PMOS transistors with the robust fault protection features of diodes. Ideal diodes provide reverse current blocking, enabling true power OR-ing functionality when multiple sources are present. This makes them highly effective in redundant power systems or applications requiring seamless power switching.

Figure 3. Power Management with Ideal Diode
Figure 3. Power Management with Ideal Diode

Ideal diodes have a significantly lower forward voltage drop than Schottky diodes, which reduces power dissipation and heat generation, thereby enhancing overall system efficiency. Additionally, their low reverse leakage current helps minimize energy loss during standby or low-power operation, which is vital in battery-powered applications.

What the data shows:

  • Traditional Schottky diodes offer fast switching and low forward voltage drop, but they still cause significant power loss and heat generation, especially at higher currents.
  • PMOS transistors improve efficiency but lack reverse current blocking, which limits their use in systems with multiple power supplies or in priority ORing configurations.
  • Integrated ideal diodes combine the advantages of Schottky diodes and MOSFETs by offering low forward voltage drop and reverse current blocking. This enables efficient, scalable power architectures in systems with multiple supplies, including applications like redundancy and priority ORing.

Key Takeaways:

  • Nexperia’s NID5100 and NID1100 integrated ideal diodes offer very low forward voltage drop, reverse current blocking, low leakage, and smart features—delivering excellent performance across a wide range of applications, including IoT systems, CO detectors, gas meters, and battery backup systems.

Want the full technical breakdown, test data, and design recommendations?

Read the full whitepaper to explore Nexperia’s findings in detail